2024-08-28 02:44 AM - last edited on 2024-08-28 06:50 AM by Peter BENSCH
Hello. im currently using the EVAL-RHF1201V2 and would like some help setting it up to properly measure dynamic characteristics. Particularly regarding the RPOL resistance and for a sampling frequency of 40 Mbps and a differential AC input from 1 MHz to 10 MHz with a max amplitude of 2Vpp.
I also tried to apply the recommendations in the datasheet (fine = 15MHz and FS = 50 Mbps) in order to measure dynamic performance but I am far from obtaining them.
Can someone help me please?
2024-08-28 06:49 AM
Welcome @Mo9, to the community!
the EVAL-RHF1201V2 is a tool from the aerospace sector. As the community is primarily intended for mutual help between end users, nobody will be able to help you here.
However, I'd recommend you create a personal ticket with Online Support OLS.
Good luck!
Regards
/Peter