cancel
Showing results for 
Search instead for 
Did you mean: 

Can USB_clk pin of STR9 used as GPIO even USB function enable?

hg-chen
Associate II
Posted on January 09, 2008 at 09:12

Can USB_clk pin of STR9 used as GPIO even USB function enable?

2 REPLIES 2
hg-chen
Associate II
Posted on May 17, 2011 at 09:49

Can USB_clk pin of STR9 used as GPIO even USB function enable?

and the USB 48MHz is from internal clock!

16-32micros
Associate III
Posted on May 17, 2011 at 09:49

Hi Kuni,

Yes, you can ;-) Looking on Table 5 (Device Pin Description) in the STR91xFA datasheet : the default Input/output function of Pin 2.7 is standard GPIO. Hope this clarifies.

STOne-32 :-)

[ This message was edited by: STOne-32 on 09-01-2008 13:43 ]