2018-11-16 6:23 AM
With version 2.6.2b I was selecting my USB to serial converter using the "non hybrid" definition. Now with 2.7.1 I only see the "Hybrid" definition and it can't connect.
"[2018/11/16 15:21:17]: SPC5 Flash Programmer 2.7.1 - Start connection: Target:SPC564B74 - External crystal: 40MHz - Interface: UCUART::HybridCom/1/UART
[2018/11/16 15:21:20]: An error occured during plugin downloading via BAM/BAF
[2018/11/16 15:21:20]: Connection end.
"
2018-11-28 2:18 AM
Hello Aurelien ,
Do you use SPC564B74 Discovery or Minimodule ?
i am checking the issue
Best regards
Erwan
2018-11-28 2:25 AM