2017-03-06 12:26 PM
Hello,
Trying to make a workaround for the flash-not-ready-after-leaving-power-saving problem, I am placing the below function in a section which goes into the .data section:
__attribute__ (( __section__ ('halt'))) void halt0(void)
{ ME.HALT0.B.CFLAON = ME.RUN[0].B.CFLAON = 1; ME.HALT0.B.DFLAON = ME.RUN[0].B.DFLAON = 1; ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_HALT0) | SPC5_ME_MCTL_KEY; ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_HALT0) | SPC5_ME_MCTL_KEY_INV; while(ME.GS.B.S_MTRANS); ME.RUN[0].B.CFLAON = 3; ME.RUN[0].B.DFLAON = 3; ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_RUN0) | SPC5_ME_MCTL_KEY; ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_RUN0) | SPC5_ME_MCTL_KEY_INV; while(ME.GS.B.S_MTRANS);}Calling this function from code in the .text segment cause the linker to fail with the message
relocation truncated to fit: R_PPC_VLE_REL24 against symbol `halt0' defined in flop section in arch/spc560/halt0.o
The exact reason for this error is not clear to me, as it is quite cryptic.
However - and this is the strange part - if I adjust the function and take out some code, the object compiles and links just fine. For example, remove the last 3 lines, and the problem is gone.
Can anyone explain what exactly causes the error message, and if there is a workaround for this?
Solved! Go to Solution.
2017-05-03 9:58 AM
Found solution gcc documentation:
__attribute__((longcall))
does the trick
2017-03-06 12:43 PM
As a side note, I can trick the compiler in calling this function just fine like this:
volatile ptrdiff_t n = 0;
void (*fn)(void) = halt0 + n; fn();2017-03-08 8:57 AM
Hello Gert ,
it seems to be a too long jump
https://gcc.gnu.org/bugzilla/show_bug.cgi?id=61972
Did you use Freegcc Vle ?
Could you send me your compilation directive ?
Do you use optimization level ?
There is a post along that.
https://gcc.gnu.org/bugzilla/show_bug.cgi?id=61972
Best regards
Erwan
2017-03-09 2:38 AM
The jump itself should be no problem for the cpu, but it seems that the linker is confused trying to fix up the relocation.
Relevant compiler flags:
powerpc-eabivle-gcc
-O2-falign-functions=16-msoft-float-Wno-pointer-to-int-cast-mcpu=e200z0-meabi-msdata=none-mregnames-mvle-mno-speCompiler is powerpc-eabivle-gcc (GCC) 4.9.2 20141030, linker is GNU ld (GNU Binutils) 2.24.90.20141014
My workaround to calculate the function address at runtime using a volatile trick does not work when optimization is disabled (-O0), in this case the same error is reported.
2017-05-03 9:58 AM
Found solution gcc documentation:
__attribute__((longcall))
does the trick