2017-04-19 10:24 AM
Hi All,
I just got a SPC5-UDESTK-eval to flash a SPC560B miniboard. I am using UDE STK 4.8 but for some reason it tries to connect via FTDI instead of JTAG. Is there any configuration I should change? I am running from Windows 10 and the SPC5-UDESTK drivers looks properly installed. Should I change any jumper in the board?
2017-04-19 12:52 PM
OK, so just found the issue. Chip legs were bended and not doing a proper connection.
The UDE STK error logs are very confusing. If you run into the same issue consider the chip status.
2017-04-24 6:09 AM
Hello ,
Good ;)
SPC5-UDESTK (PLS UDE 4.8) is managed by FTDI-USB drivers;
Best regards
Erwan