cancel
Showing results for 
Search instead for 
Did you mean: 

FlexRay SPC56EL70L5

David Staffenberger
Associate III
Posted on August 08, 2017 at 08:29

Hello community,

I am asking myself if there is actually anyone running FlexRay on the SPC56EL70L5 Board?

I am currently stuck in the wakeup process (I think that is where I am stuck), because the wakeup pattern does not get send. Does anyone have any experience with that?

Thanks in advance.

Best Regards,

David

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
Posted on August 11, 2017 at 12:49

Hello David,

1.)

Node B should be

integration_listen

state just like you said. I think you left the part in your code for Node B which set the controller into POC:allow coldstart.

Example:

/***********************************************/
// flexray_allow_coldstart(&Flex1);
 sysWaitMilliseconds(90UL);
 flexray_start_communication(&Flex1);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

If I dont include the allow_coldstart part the POC ends in the

integration_listen state:

0690X00000607Y1QAI.png

2.)

Could that be that the

FID and HCRC are from different frames sent by different nodes? You should try to configure to usethe keyslot as a startup / sync frame so you know what do you need to see on the scope.

3.)

Accordint to the specification: A TT-L coldstart node always finishes the startup after six cycles. What I still dont know how the controller knows that he is a TT-D or a TT-L coldstart node. I think the reason that your Noda A does not stop transmitting his sync frames is because he think that he is a TT-D cs node. Here is the image of the TT-D coldstart startup:

0690X00000607pjQAA.png

I will give you an update if I find anything out.

As for the rest I am still trying to get the node to send some sync frames soI havent had the chance to test the rest of the protocol

Regards,

Marcell

Ps: Alternatively, I cluster with two coldstart nodes also should be able to start the communication completely. Pay attention to the correct configuration of the startup frames to avoid collisions.

Edit:

Just guessing but it might work:

  1. Set thegClusterDriftDamping to 0 (zero)

  2. A TT-L coldstart node needs to act like the cluster contains two coldstart nodes -> a non-sync node shouldnt recognise the difference between a TT-D and a TT-L cluster. So your coldstart nodes need to transmit two startup frame in each cycle so it would look like there is two coldstart node on the channel. For this you should:

    • SetpTwoKeySlotMode to TRUE

    • Set the ID for the second keyslot (Assuming your first keyslot id's is 1, setting it to 2 shall work)

    • And the action point offset need to calculate in a different way. What is your value for the action point offset?

Edit 2:

It looks like only FlexRay Protocol Specification 3.0 supports the TT-L cluster type and the SPC56xx microcontroller series implements the 2.1 version so you should ignore what i said about the single node startup.

From the spec.:

In clusters consisting of less than three nodes, each node shall be a coldstart node. Each startup frame shall also be a sync frame; therefore each coldstart node will also be a sync node. The parameter gColdStartAttempts shall be configured to be at least two. At least two fault-free coldstart nodes are necessary for the cluster to start up.

Posted on August 16, 2017 at 08:44

Hello Marcell,

I am really amazed how detailed your answers are, thank you so much for that.

1)

Actually, I did not leave it in there, but I realized that I have to disable pKeySlotUsedForStartup on my non-coldstart node but I am still not in integration_listen. I also did not realize that with 2 nodes both of them have to be coldstart nodes. I misunderstood the specification at this point - will try if it works of they both are coldstart nodes.

2)

I think that the sync frames came from both boards. I am not 100% sure but I think that there should be everything correct - I guess there was some misunderstanding on my side. Although I am not sure why it does not show my configured pKeySlotHeaderCRC?

3)

At this point I am a little bit clueless what TT-L or TT-D means and I cannot find anything in the specification.

But I have seen this timing diagram - that is why I am a little bit confused because I am not reaching those states plus I think that some of those startes cannot be seen on the debugger because they happen 'so fast'.

The configuration I got was from a sample program NXP offers with their MPC5 boards becasue they should be pretty similar to my controller as far as I know. But it seems that there are some faults in the configuration or at least I already found a constraint violation. Is there any  chance that you could provide some sort of super basic configuration for two nodes? It is kind of hard to configure all those parameters without any help or tools.

My actionPointOffset is 3 and the drift dampening is 1. 

Can I simply chance one of those parameters?

Thank you so much for your help - I will try some of your suggestions and will edit this answer.

Best regards, 

David.

EDIT 1:

I just double checked - and I actually forgot to remove the coldStartAllowed part, now I am in integration listen.

Now I just ran into an issue that one of the controller seems not to work properly, I am not able to load any programs onto it, but that is a different issue.

Posted on August 16, 2017 at 09:57

Hello David,

Yes I mixed up a little bit the version numbers and I wrote a few false thing about the startup, so to clear it up:

  • The startup needs at least two coldstart nodes, one leading and one following. The following coldstart node should be able to see that the coldstart process has been started on the channel. (maybe delay a bit the transition to the startup state on the following node should work?) The following node should end in the Coldstart Join state before reaching the normal active state
  • The two nodes need to have different key slot IDs obviously so they would not be transmitted in the same slot. Keep in mind that what you see on the scope is containing the coding sequences (TSS, FSS, BSS), so if you want to decode the frame segments exclude those.0690X00000607fbQAA.png
  • For the configuration I use a sample from the Nxp guys as well.

Best Regards

 Marcell

David Staffenberger
Associate III
Posted on August 28, 2017 at 10:32

Hello Guys, little update:

I have now checked a few things and I realized something. 

I configured the coldstart_attempts to be 10, but in the register FR_PSR1 the field REMCSAT indicates that I have 19 attempts left. Any experience?

EDIT:

Is it at this point actually important that the message buffers are configured correctly?

Best Regards,

David

David Staffenberger
Associate III
Posted on August 29, 2017 at 14:24

I was finally able to bring the bus into POC:normal_active state. It was my fault.

I built a struct for the 30 PCR registers where all the configuration parameter go. These registers are all 16-bit long but I made a mistake which resulted the PCR11 to be longer than 16 bit and therefore all the following parameter where shifted to the back. 

Thank you to both of you for your time and help! I really appreciate it.

Best Regards,

David.