2018-08-02 2:36 AM
2018-08-21 1:27 AM
Yes, the primary side of STGAP1AS can work at either 3.3 V and 5 V supply voltage (VDD). Please refer to figure 3 in the datasheet for the proper connection to be used in each case.
The login input thresholds Vil and Vih are (1/3)*VDD and (2/3)*VDD respectively.
Tha nks and regards
Michele
2019-04-02 10:50 PM
Hello,
I am facing SPI communication issue with STGAP1AS.
I am using EVALSTGAP1AS board with STM8S105C6 discovery kit.
I am not getting right value with SPI read register.
Below is SPI Init. As mentioned in datasheet CPHA = 1 and CPOL = 0
SPI_Init(SPI_FIRSTBIT_MSB, SPI_BAUDRATEPRESCALER_16, SPI_MODE_MASTER, SPI_CLOCKPOLARITY_LOW, SPI_CLOCKPHASE_2EDGE, SPI_DATADIRECTION_2LINES_FULLDUPLEX, SPI_NSS_SOFT,(uint8_t)0x07);
Read Register Routine.
u8 stGAP_ReadReg(u8 addr)
{
u8 TxData[4], TxCount = 0;
TxData[TxCount++] = addr;
TxData[TxCount++] = CRC_BYTE;
TxData[TxCount++] = NOP_BYTE;
TxData[TxCount++] = CRC_BYTE;
GPIO_WriteLow(SPI_CS_PORT, SPI_CS_PIN);
MSDelay(1);
for(u8 i = 0; i < TxCount; i++)
{
while (SPI_GetFlagStatus(SPI_FLAG_TXE)== RESET);
SPI_SendData(TxData[i]);
while (SPI_GetFlagStatus(SPI_FLAG_RXNE) == RESET);
RxData[i] = SPI_ReceiveData();
}
GPIO_WriteHigh(SPI_CS_PORT, SPI_CS_PIN);
MSDelay(1);
return RxData[2];
}
#define CGF1 0x0C
#define CGF2 0x1D
#define CGF3 0x1E
#define CGF4 0x1F
#define CGF5 0x19
Config[0] = stGAP_ReadReg(0xA0 | CGF1);
Config[1] = stGAP_ReadReg(0xA0 | CGF2);
Config[2] = stGAP_ReadReg(0xA0 | CGF3);
Config[3] = stGAP_ReadReg(0xA0 | CGF4);
Config[4] = stGAP_ReadReg(0xA0 | CGF5);
But This Reads
CFG1 = 0xAC
CFG2 = 0xBD
CFG3 = 0xBE
CFG4 = 0xBF
CFG5 = 0xB9
I have tried different ways but all time gives same result.
Whats wrong in my code?