cancel
Showing results for 
Search instead for 
Did you mean: 

What are the SW & HW tools to acess CAN bootloader on SPC5 eval boards

ZBen .11
Associate

Hello community,

An automotive client that i'm working with wants to devolope his own bootloader basing on ST bootloader on SPC5 product. my mission is to validate this bootloader on SPC5 eval bord of ST.So , im asking if there is a specific HW and SW tools to validate CAN UDS bootloder. Also any documentation about CAN bootloader could help

Thinks in advance

Farmer ST engineer

Zied ben Amira

1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Hello,

open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,

read the section M_CAN download protocol.

Regards,

Giuseppe

View solution in original post

2 REPLIES 2
Giuseppe DI-GIORE
ST Employee

Hello,

open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,

read the section M_CAN download protocol.

Regards,

Giuseppe

Thanks Giuseppe,

I was hoping there were something already done by ST ....

But ... can I configure CAN as bootloader (SPC570Sxx Firmware Updater Component) and then 

I will have to create only an host application to download the firmware via CAN?

Fabio