cancel
Showing results for 
Search instead for 
Did you mean: 

StellarStudio using Jlink Debug issue

BillyWu
Associate

Hi,

I using the GDB SEGGER J-link with JTAG debug, and stuck in 

"Setting breakpoint @ address 0x24001362, Kind = 2, Type = THUMB, BPHandle = 0x0001
Starting target CPU..."

Please help, thanks~

 

 

 

3 REPLIES 3
Erwan YVIN
ST Employee

Hello ,

Could you detailed your issue ?

On which platform you have the issue SR5 / SR6 ?

        Best Regards

                           Erwan

Hi Erwan,

I use SR5E1 and debug with GDB SEGGER J-link with JTAG in stellar studio.

BillyWu_0-1724897798050.png

 

I using stellarLink can debug successfuly, but can not debug in nvm,

I have changed the makefile CONFIG_TARGET_MEMORY ?= nvm, and the debug setting unselect  debug in ram.

After debug, programs don't stop on main and even don't run.

BillyWu_1-1724898189016.png

 

 

Hi,

Now I can use Jlink to debug the project with ram, but I can not use nvm. Below is the log of debug, just stack in Starting target cpu... I use SR5E1E7, please help, many thanks~

BillyWu_0-1724923009957.pngBillyWu_1-1724923035057.png

BillyWu_2-1724923055129.png