cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5x pinout

GMG
Associate III

Hi, where can I find microcontroller pinout?

I miss something? I can't find spc5 pinouts in datasheets, where are these resources?

Best regards​

1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Hello,

for each SPC5 MCU pinout description is available in a specific technical note.

See the MCU specific documentation page.

For example, SPC58EC pinout is available in Technical Note TN1260 (link)

Download the MCU specific I/O definition technical note, it is in pdf format,

then the I/O pinout file is attached to the pdf as spreadsheet file.

Regards.

View solution in original post

3 REPLIES 3
Giuseppe DI-GIORE
ST Employee

Hello,

for each SPC5 MCU pinout description is available in a specific technical note.

See the MCU specific documentation page.

For example, SPC58EC pinout is available in Technical Note TN1260 (link)

Download the MCU specific I/O definition technical note, it is in pdf format,

then the I/O pinout file is attached to the pdf as spreadsheet file.

Regards.

thanks, opening the pdf from the browser it is not possible to see attachments and therefore I could not understand where they were.

Giuseppe DI-GIORE
ST Employee

Hello,

please do not open the file in a browser, download it instead.

Open with a pdf viewer, for example Acrobat Reader

Open the left menu and click on the paperclip.

0693W00000Kaim1QAB.pngRegards,