cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio Compatibility

asn
Associate II

I am currently using an SPC56P chip for my application. But I do not have an debugger probe for it which is compatible with SPC5Studio. So my question is: 

1. Is SPC5-UDESTK-EVAL the only debugger probe that is compatible with SPC5Studio ? Or are there any other SPC5Studio compatible debugger ?

2. Is there any other IDE, that will allow to use the Segger J-Link as debugger for SPC56P chip ? 

3. The webpage of SPC5-UDESTK-EVAL suggests it being NRND (not recommended for new design), so is there a newer model available instead of it for SPC5Studio ? 

 

I have tried SPC5Studio and AutoDevKitStudio and I think both are not compatible with J-Link. 

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

SPC5Studio and AutoDevKitStudio do not support SPC56 Family with :

https://www.segger.com/supported-devices/st/spc56

i recommend to use https://www.st.com/en/development-tools/spc5-udestk.html

                Best regards

                           Erwan

 

 

 

 

 

View solution in original post

3 REPLIES 3
Erwan YVIN
ST Employee

SPC5Studio and AutoDevKitStudio do not support SPC56 Family with :

https://www.segger.com/supported-devices/st/spc56

i recommend to use https://www.st.com/en/development-tools/spc5-udestk.html

                Best regards

                           Erwan

 

 

 

 

 

Also another follow up question with respect to AEK-MCU-SPC5LNK, When will it be ready to use with SPC56 ? Is there any estimated time ?

Erwan YVIN
ST Employee

Hello ,

AEK-MCU-SPC5LNK (FTDI Chipset)should work with OpenOCD (SPC58 only)

AEK-MCU-SPC5LNKU (FTDI Chipset) should work with UDE PLS (SPC56,SPC57 and SPC58)

         Best Regards

                      Erwan