cancel
Showing results for 
Search instead for 
Did you mean: 

SPC574K

Shiyu
Associate

微信图片_20240603164008.jpg微信图片_20240603163958.jpg

I am working on the development of SPC574K chip, but the debugger cannot connect with the chip successfully. When the chip is powered on, the crystal waveform is the first picture, which is normal. When I press the reset button or the connect button in the computer debugging software, the waveform of the crystal oscillator becomes the second picture. I want to know if the debugger's inability to connect to the chip is the reason, and why the reset makes the crystal oscillator work incorrectly.

1 REPLY 1
Erwan YVIN
ST Employee

Hello ,

Which debugger do you use ?

           Best Regards

                            Erwan