cancel
Showing results for 
Search instead for 
Did you mean: 

SPC563M64L5 and SPC560P50L5 microcontrollers pin compatible

Dariush.Tsh
Associate II

Are the SPC563M64L5 and SPC560P50L5 microcontrollers pin compatible?

I mean, can two microcontrollers be assembled instead of each other?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

OK, Tkanks...