2021-12-05 10:20 PM
Are the SPC563M64L5 and SPC560P50L5 microcontrollers pin compatible?
I mean, can two microcontrollers be assembled instead of each other?
Solved! Go to Solution.
2021-12-05 11:56 PM
There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.
Regards
/Peter
2021-12-05 11:56 PM
There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.
Regards
/Peter
2021-12-06 12:00 AM
OK, Tkanks...