2019-01-04 05:40 AM
Hi ST experts,
I started with SPC560B50L3 and I am using SPC5Studio 5.8. I have problem with eMIOS0 configuration (ch1-ch7) as PWM outputs.. I use PinMap editor and i configured the pins as eMIOS0 output (eMIOS0 ch1-ch7, eMIOS0 ch9-ch13 and eMIOS0 ch20-ch21).
I can configure eMIOS0_group0 (ch9-ch15) and eMIOS0_group1 (ch17-ch23) but cannot configure eMIOS0 ch1-ch7 as PWM, why?
I saw into RM0017 document on figure 250 channel configuration. How i understand it.. there are 6 PWM output groups.. 3 groups for eMIOS0 and 3 groups for eMIOS1, is not it? For package, which i use, i can used only eMIOS0 (LQFP100) and i need to use all three groups of eMIOS0 for PWM outputs.
But via Low Level Driver configuration, i can configure only two groups of eMIOS0 as PWM output.
I use SPC560B54L5 and i saw in document RM0037 (figure 357) very similar channel configuration as for SPC560B50L3. I used the MCU with SPC560B-DIS board and there is no problem configured all 3 groups of eMIOS0 as PWM output.
Please, can you explain me what i do wrong?
Thank you for help
Solved! Go to Solution.
2019-01-10 01:59 AM
Hello Vit ,
It is the driver implementation .
You need to update the driver in order to support it.
not to use the component.
Best regards
Erwan
2019-01-10 01:59 AM
Hello Vit ,
It is the driver implementation .
You need to update the driver in order to support it.
not to use the component.
Best regards
Erwan