cancel
Showing results for 
Search instead for 
Did you mean: 

SPC56 aborted FCCU operation

DaveJ
Associate

I want to clear the FCCU flags on my SPC56 chip. From the test application generated by SPC5Studio, I have the following code:

static void spc_clear_fccu_rgm(void) {

/* FCCU CF errors clearing.*/
/* Clear FCCU CF Status Register0 errors.*/
FCCU.CFK.R = 0x618B7A50UL;
FCCU.CFS[0].R = 0xFFFFFFFFUL;
while (FCCU.CTRL.B.OPS != 3U) {
}

/* Clear FCCU NCF Status Register0 errors.*/
FCCU.NCFK.R = 0xAB3498FEUL;
FCCU.NCFS[0].R = 0xFFFFFFFFUL;
while (FCCU.CTRL.B.OPS != 3U) {
}

/* RGM errors clearing.*/
RGM.FES.R = 0xFFFFU;
RGM.DES.R = 0xFFFFU;
}  

However, when I execute this on the chip, it gets stuck on the first while loop, since the OPS field is 0x2 (aborted). The reference manual (RM0032) states that:

The ABORT response occurs in the following cases:
– wrong access (missing or wrong key) to the FCCU_CFS register (clear operation OP11)
– wrong access (missing or wrong key) to the FCCU_NCFS register (clear operation OP12)
– wrong access (missing or wrong key) to the FCCU_CTRL register (OP1, OP2, OP16
operation)
– OP1 (CONFIG command) execution when FCCU state ≠ NORMAL or configuration locked
– OP20–OP30 (RESERVED operations) execution

 

Which one is the likely cause in my case? I would have expected the auto-generated example code to work without errors. Could there be any other causes that are not mentioned in the manual? 

0 REPLIES 0