cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 Studio v6.0 - warning/issue "Type 'uint32_t' could not be resolved

RatheeshT
Associate II

I have installed SPC5 Studio version 6.0 on my Windows 10 PC and compiled sample code.

When compiling the project , i got below warning/issue "Type 'uint32_t' could not be resolved"

Q1: Can you give the solution for this?

10 REPLIES 10

Thank you so much for the answer. It really helped. 

For others to refer to his solution, you can refer to the below screenshot. |

I added only one directory and it resolved: 

 

C:/SPC5Studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/lib/gcc/powerpc-eabivle/4.9.4/include

 

asn_0-1724334471986.png