cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 studio project problems when compiling with -Os

davedave95
Associate III
Posted on February 09, 2017 at 17:10

When compiling a SPC5 studio generated demo program with -Os to optimize on size, the resulting code stalls during initialisation. in eirqInit() the loop

  while (eirqconf[i].eirqNumber != -1) {

never terminates when the eirqconf[] table has no entries except for the terminator record where irq is set to -1

  const eirq_config eirqconf[]={

    {-1,0,0,0,NULL}

  };

Is this a known issue, can anyone reproduce?

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Erwan YVIN
ST Employee
Posted on February 09, 2017 at 17:26

Hello Gert ,

could you confirm your test application tested ?

Do you use ppc-freevlvle-eabi or hightec gcc ?

i will check with my board.

to debug this issue , you should focus your assembly code not C code.

you should add --save-temps and check your .s file 

      Best Regards

                   

                     Erwan

davedave95
Associate III
Posted on February 09, 2017 at 17:29

Using the ppc-freevle-eabi 4.9.2 compiler. I'm currently trying to reproduce by generating a minimal example function which shows the same behaviour.

davedave95
Associate III
Posted on February 09, 2017 at 17:48

Minimal snippet to reproduce.

The following never terminates:

#include <stdint.h>

volatile int store1, store2;

int8_t fs[] = { -1 };

void bug(void)

{

        uint8_t i = 0;

        while (fs[i] != -1) {

                uint8_t v = (uint8_t)fs[i];

                store2 = v;

                store1 = fs[i];

                i++;

        }

}

However, removing the line 'store1 = fs[i]' or 'store2 = v' will change the behaviour so that the loop terminates.

Assembly:

  0:   70 e0 e0 00     e_lis   r7,0

   4:   70 c0 e0 00     e_lis   r6,0

   8:   71 20 00 00     e_li    r9,0

   c:   1c e7 00 00     e_add16i r7,r7,0

  10:   1c c6 00 00     e_add16i r6,r6,0

  14:   7d 47 48 ae     lbzx    r10,r7,r9

  18:   7d 48 07 74     extsb   r8,r10

  1c:   18 28 ac ff     e_cmpi  cr1,r8,-1

  20:   7a 16 00 18     e_beq   cr1,38 <bug+0x38>

  24:   75 4a 06 3f     e_rlwinm r10,r10,0,24,31

  28:   19 29 80 01     e_addi  r9,r9,1

  2c:   55 46 00 00     e_stw   r10,0(r6)

  30:   75 29 06 3f     e_rlwinm r9,r9,0,24,31

  34:   79 ff ff e0     e_b     14 <bug+0x14>

  38:   00 04           se_blr
davedave95
Associate III
Posted on February 09, 2017 at 20:10

And even simpler code:

void boom(int a, int b)

{

        printd('%d %d\n', a, b);

}

int8_t fs = -1;

void bug(void)

{

        if (fs != -1) {

                boom((uint8_t)fs, fs);

        }

}

resulting in

bug:

.LFB2:

        .loc 1 15 0

        .cfi_startproc

        .loc 1 16 0

        e_lis %r9,.LANCHOR0@ha

        e_lbz %r3,.LANCHOR0@l(%r9)

        se_extsb %r4

        e_cmpi %cr1,%r4,-1

        e_beq %cr1,.L2

        .loc 1 17 0

        se_extzb %r3

        .loc 1 19 0

        .loc 1 17 0

        e_b boom
davedave95
Associate III
Posted on February 09, 2017 at 21:34

Sorry to keep spamming my own topic, but things are getting more and more weird. The following snippet shows wrong behaviour with -O2, but not with -Os:

signed char fs = -1;

void boom(int a)

{

        printd('boom %d %d\n', (int)fs, (int)a);

}

void bug(void)

{

        if (fs != -1) {

                boom((unsigned char)fs);

        }

}

The expression in the 'if' is handled as if it is true, and the output of the program is

boom 1 255

The beaviour of the program is not stable: if 'signed char fs' is declared volatile, it behaves as expected.

I feel that the integer promotion in the if expression seems to mess up, but I can't get my finger around it.

I found some references about ppc being kind of special considering the 'char' type, which is unsigned by default instead of signed on this architecture, although I'm not sure if that is relevant for this case.

Posted on February 10, 2017 at 10:35

Hello Gert ,

It seems to be a compiler issue.

i am contacting thecompiler team.

for your information, It is not the last version of the compiler

you can try with the last version 10/12/2016 from NXP website

https://community.nxp.com/docs/DOC-333045

by updating ,c:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_1.0.0.201611101103

anyway, you can force

__attribute__((optimize('-O0'))) 
�?
�?�?�?�?�?

I have created a ticket for this issue.

Best regards

Erwan

Posted on February 10, 2017 at 10:55

Thank you for the confirmation. I will try the updated compiler when possible - the NXP site is not available at this moment:

We are unable to complete your software download request at this time due to a system outage. Please try your download at a later time. We apologize for the inconvenience.

It has been like this for a few days already, unfortunately.

Posted on February 13, 2017 at 11:55

Same results with this compiler.