cancel
Showing results for 
Search instead for 
Did you mean: 

Slave Mode Setting for DSPI1 in SPC560D40L1 Chip

Posted on April 11, 2017 at 09:31

Hi Everyone, I am using SPC560D40L1 micro controller and trying to configure DSPI1 to be in slave mode. I am using SPC5studio to make the configuration. I have set pin directions and OBE and IBE along with WPS and WPE configurations for the CS and changed directions for the clock and CS, I have made use of the CS0_1 pin as per the datasheet for enabling slave mode. Is there any other settings that i need to take care of? When i see the resgister settings of DSPI 1  during code execution it shows the channel is always in master mode. Does anyone know how i need to set the slave mode for the DSPI channel? Thanks in advance Preetha.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
Erwan YVIN
ST Employee
Posted on April 12, 2017 at 15:57

Hello , 

Did you set the corresponding MSTR to 0 ?

MSTR

Master/slave mode select

Configures the DSPI for master mode or slave mode.

0 DSPI is in slave mode

1 DSPI is in master mode

Anyway , for the pinmap point of view you should configure 

In slave mode, the CS0_x signal is a slave select input signal that allows an SPI master to

select the DSPI as the target for transmission. CS0_x must be configured as input and

pulled high. If the internal pullup is being used then the appropriate bits in the relevant

SIU_PCR must be set (SIU_PCR [WPE = 1], [WPS = 1]).

         Best regards

                         Erwan