cancel
Showing results for 
Search instead for 
Did you mean: 

Recommendation of PART no of MCU with datasheet which will meet automotive standard

Nabanita_23
Associate

I need one part no of MCU which will meet automotive standard and have MCU 32-bit ARM Cortex M0+ RISC 512KB Flash 2.5V/3.3V 32-Pin, 512 KB flash Memory, 64 MHz clock rate and operating temperature is -40 to 125 °C.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Nabanita_23, to the community!

No device with your specification and Automotive certification is currently available.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.