cancel
Showing results for 
Search instead for 
Did you mean: 

EVAL-L9788 with SPC57K-Line MCU

angela_
Associate
Hello,

I am working on SPC57K-Line MCU with IC L9788. I want to use also GUI to configure and control L9788 through the MSC bus. But I always see this error "Failed to reset MONACO". I tested COM port and UART connection and all connections are correct and working. In website, I saw the L9788 can be connected to the SPC563M-DISP directly and GUI can be used. 

angela__0-1710943379950.png

Can I use this GUI with SPC57K-line board? If yes, could you please provide elf file? Because the elf file given with GUI folder is for SPC563M-DISP board. (like STSW-L9788.elf)

Btw, if there are any preconditions to receive message from l9788, please inform me.

Thank you

 

 

 

 

 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
0 REPLIES 0