cancel
Showing results for 
Search instead for 
Did you mean: 

irqIsrEnable Debug Crash

PChia.2237
Senior

Hi,

i have spc560p50l5 if i enable irqIsrEnable(); in debug it crash. (no codes execuded after).

If i comment //irqIsrEnable(); debug works, but osal not starts.

In assembly code of swirq_enable there are a lot OF_SE_ILLEGAL

0x400001E8 00 00    SE_ILLEGAL  

0x400001EA 00 00    SE_ILLEGAL

 /**

 * @brief  Enable software IRQ.

 *

 * @param[in] irq  software irq number

 * @param[in] prio interrupt priority

 * @param[in] core core to dispatch interrupt

 *

 * @sa

 * INTC_PSR_CORE0, INTC_PSR_CORE1, INTC_PSR_CORE2,

 * swirq_disable

 *

 * @notapi

 */

void swirq_enable(uint8_t irq, uint8_t prio, uint32_t core) {

 irq &= 0x1FU;

 INTC_PSR((irq)) = INTC_PSR_ENABLE(core, prio);

0x00000014 78 00 01 5C E_B    _boot_address (0x00000170)  

_disablewatchdog:

0x00000018 70 9F E7 F3 E_LIS   R4,0xFFF3

0x0000001C 70 90 C0 00 E_OR2I  R4,0x8000

0x00000020 70 78 05 20 E_LI   R3,0xC520

}

0x00000024 54 64 00 10 E_STW   R3,0x10(R4)

0x00000028 70 7B 01 28 E_LI   R3,0xD928

0x0000002C 54 64 00 10 E_STW   R3,0x10(R4)

0x00000030 70 7F E7 00 E_LIS   R3,0xFF00

}

0x00000034 70 60 C0 0A E_OR2I  R3,0xA

0x00000038 54 64 00 00 E_STW   R3,0x0(R4)

0x0000003C 00 04    SE_BLR   

0x0000003E 44 00    SE_OR   R0,R0

_coreinit:

0x00000040 7C 00 02 78 XOR    R0,R0,R0

0x00000044 7C 21 0A 78 XOR    R1,R1,R1

0x00000048 7C 42 12 78 XOR    R2,R2,R2

0x0000004C 7C 63 1A 78 XOR    R3,R3,R3

0x00000050 7C 84 22 78 XOR    R4,R4,R4

0x00000054 7C A5 2A 78 XOR    R5,R5,R5

0x00000058 7C C6 32 78 XOR    R6,R6,R6

0x0000005C 7C E7 3A 78 XOR    R7,R7,R7

0x00000060 7D 08 42 78 XOR    R8,R8,R8

0x00000064 7D 29 4A 78 XOR    R9,R9,R9

0x00000068 7D 4A 52 78 XOR    R10,R10,R10

0x0000006C 7D 6B 5A 78 XOR    R11,R11,R11

0x00000070 7D 8C 62 78 XOR    R12,R12,R12

0x00000074 7D AD 6A 78 XOR    R13,R13,R13

0x00000078 7D CE 72 78 XOR    R14,R14,R14

0x0000007C 7D EF 7A 78 XOR    R15,R15,R15

0x00000080 7E 10 82 78 XOR    R16,R16,R16

0x00000084 7E 31 8A 78 XOR    R17,R17,R17

0x00000088 7E 52 92 78 XOR    R18,R18,R18

0x0000008C 7E 73 9A 78 XOR    R19,R19,R19

0x00000090 7E 94 A2 78 XOR    R20,R20,R20

0x00000094 7E B5 AA 78 XOR    R21,R21,R21

0x00000098 7E D6 B2 78 XOR    R22,R22,R22

0x0000009C 7E F7 BA 78 XOR    R23,R23,R23

0x000000A0 7F 18 C2 78 XOR    R24,R24,R24

0x000000A4 7F 39 CA 78 XOR    R25,R25,R25

0x000000A8 7F 5A D2 78 XOR    R26,R26,R26

0x000000AC 7F 7B DA 78 XOR    R27,R27,R27

0x000000B0 7F 9C E2 78 XOR    R28,R28,R28

0x000000B4 7F BD EA 78 XOR    R29,R29,R29

0x000000B8 7F DE F2 78 XOR    R30,R30,R30

0x000000BC 7F FF FA 78 XOR    R31,R31,R31

0x000000C0 70 88 E0 00 E_LIS   R4,0x4000

0x000000C4 70 80 C0 00 E_OR2I  R4,0x0

0x000000C8 70 A8 E0 00 E_LIS   R5,0x4000

0x000000CC 70 B4 C0 00 E_OR2I  R5,0xA000

.cleareccloop:

0x000000D0 7C 04 28 40 CMPL   0x0,0x0,R4,R5

0x000000D4 E0 06    SE_BGE  .cleareccend (0x000000E0)  

0x000000D6 1A 04 09 00 E_STMW  R16,0x0(R4)

0x000000DA 18 84 80 40 E_ADDI  R4,R4,0x40

0x000000DE E8 F9    SE_B   .cleareccloop (0x000000D0)  

.cleareccend:

0x000000E0 70 60 02 01 E_LI   R3,0x201

0x000000E4 7C 75 FB A6 MTSPR   0x3F5,R3

0x000000E8 00 04    SE_BLR   

0x000000EA 44 00    SE_OR   R0,R0

_ivinit:

0x000000EC 70 60 E0 06 E_LIS   R3,0x6

0x000000F0 70 62 C0 00 E_OR2I  R3,0x1000

0x000000F4 7C 60 01 24 MTMSR   R3

0x000000F8 70 60 E0 00 E_LIS   R3,0x0

0x000000FC 70 62 C0 00 E_OR2I  R3,0x1000

0x00000100 7C 7F 0B A6 MTSPR   0x3F,R3

0x00000104 00 04    SE_BLR   

0x00000106 00 00    SE_ILLEGAL  

0x00000108 00 00    SE_ILLEGAL  

0x0000010A 00 00    SE_ILLEGAL  

0x0000010C 00 00    SE_ILLEGAL  

0x0000010E 00 00    SE_ILLEGAL  

.unhandled_exception:

0x00000110 78 00 00 00 E_B    .unhandled_exception (0x00000110)  

0x00000114 00 00    SE_ILLEGAL  

0x00000116 00 00    SE_ILLEGAL  

0x00000118 00 00    SE_ILLEGAL  

0x0000011A 00 00    SE_ILLEGAL  

0x0000011C 00 00    SE_ILLEGAL  

0x0000011E 00 00    SE_ILLEGAL  

_IVOR4:

0x0000012

ALSO I have

Sa 06.08.2022 14:30:46.393, Warning, Core, PpcJtagTargIntf, Unknown break cause !!!

Sa 06.08.2022 14:30:46.406, Warning, Core, CallFrame, could not read memory at 0x0000000084D9F412

Sa 06.08.2022 14:30:47.379, Warning, Core, PpcJtagTargIntf, Unknown break cause !!!

Sa 06.08.2022 14:30:47.391, Warning, Core, CallFrame, could not read memory at 0x0000000084D9F412

How can i solve this?

Thank you in advantages

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
PChia.2237
Senior

I solve change board

View solution in original post

2 REPLIES 2

Check whatever you're enabling is actually handled properly.

Perhaps stack,vector tables, ISRs, etc.

Start with simple working examples,

Review all available technical documentation for the core.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
PChia.2237
Senior

I solve change board