2019-10-15 6:03 PM
The actual situation is shown in Figure 1. I try to solve this problem in “Default Programs Editor�?,but I didn't find the “wsx�? file in Figure 2. Is there any way to solve it?
Solved! Go to Solution.
2019-10-16 6:42 AM
Hello ,
you should install PLS UDE Tool (cf Help section)
There is a tutorial inside
Best Regards
Erwan
2019-10-16 6:42 AM
Hello ,
you should install PLS UDE Tool (cf Help section)
There is a tutorial inside
Best Regards
Erwan
2020-01-10 1:01 AM
I have also done the same .but debug button is not activating.
2020-01-27 6:58 AM
Hi,
1.To execute and debug your application:
Go to C drive> SPC5STUDIO > workspace>"Project Name"> UDE> right click on "degug"> open with "UDE Visual platform"> click on check box for "always use this app to open .wsx file
2.Restart the app
3.Now in SPC5 Studio>"Execute and debug your
application" will activate
Regards,
Pradnya
2020-02-05 10:50 PM
I am able to get the path what you explained in above.
2020-10-03 10:52 AM
@Aparna i am struggling with the same thing. were you able to solve it?
@Pradnya i am not able to find UDE visual platform
2020-11-10 1:41 AM
It works only to light up the icon. Just launch UDE STK debugger, click File > Open Workspace and select 'Project\UDE\debug.wsx' file.
2020-11-12 7:35 AM
I found an offical guide by pls to integrate the UDE STK debugger to SPC5Studio. It shoud be in C:\Program Files (x86)\pls\UDE Starterkit 5.0\Help\UDEEclipsePlatform.chm