cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Memory Boot

kevin239955_st
Associate II
Posted on January 29, 2015 at 13:56

Hi

Section 6.1.1 of the SPC560x Reference Manual says that ''in order to successfully boot from flash memory, you must program two 32-bit fields into one of 5 possible boot blocks.''

I have written 0x005A005A to address 0x00000000 accordingly (on our SPC56B Discovery Kit) but neglected to program a valid 32-bit reset vector. Now the board is stuck in reset (I can't even connect the JTAG probe).

Is there any way of resolving this? Not just to ''unbrick'' the development hardware but if this were to happen ''in the field''.

Thanks

Kevin
24 REPLIES 24
Erwan YVIN
ST Employee
Posted on February 24, 2015 at 17:37

Good news ;)

Sorry for the delay ;)

kevin239955_st
Associate II
Posted on February 24, 2015 at 17:48

With the correct boot address (0x00000008) the Discovery board still does not boot without stimulus from JTAG. Is there another jumper setting somewhere that I am missing? Memory dump attached.

Thanks

Kevin

________________

Attachments :

Boot_Sector_0_Dump.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0J1&d=%2Fa%2F0X0000000ba1%2F_NDuEhStJFEdEPnUFmk4ej_6R4nuhU1wrOFesXejcuM&asPdf=false
Erwan YVIN
ST Employee
Posted on February 25, 2015 at 14:15

Hello Kevin ,

your bootaddress seems to be correct 0x00000008.

in our repository application ..but after it does not match 

in our application : 

0xE904 should be a branch into  _coreinit (0x10)

0xE959 should be a branch  _ivinit (0xBC)

After a Branch  _boot_address (0x00000130)

is it possible for you to break on the address 0x00000000 or 0x00000008 ?

is it an Application repository ?

  Best regards

            Erwan

kevin239955_st
Associate II
Posted on February 25, 2015 at 14:57

Erwan

We are not using SPC5Studio code, this is our own ''bare metal'' software (this is a high integrity avionics application).

I can break on 0x00000008 but not on 0x00000000. If I run the program using a JTAG reset (and ''Start Program Execution'' in UDE) it executes correctly. But if I remove power to the board and re-power without JTAG it does not boot from Flash as expected.

Kevin

Erwan YVIN
ST Employee
Posted on February 26, 2015 at 14:29

Hello Kevin ,

Our BOOT_ID is set to 0x015A0000

did you reset your jumper PA8 and PA9 to 0 after ''unbrick'' your discovery board ?

PA8 and PA9 to 0 means ''Flash Memory Boot by default.''

Best regards

 

                      Erwan

kevin239955_st
Associate II
Posted on February 26, 2015 at 16:54

Erwan

Our Boot Id is also now 0x015A0000.

PA8 and PA9 are back to 0 since the ''unbrickening''. I've also tried the same software on another board which is fresh in its default (factory) configuration with the same result.

If I reset the board with JTAG and then disconnect the code runs. But still if I power the board without JTAG the board looks as if it is stuck in reset.

Do you have a simple test Flash build I could try out? 

Kevin

Erwan YVIN
ST Employee
Posted on February 26, 2015 at 17:23

Hello Kevin ,

Could you try the application in SPC5Studio environment from the application wizard ?

SPC560Bxx OS-Less Test Application for Discovery (LED blinking)

Generate , Compile and debug (in order to flash)

Best regards

                      Erwan

kevin239955_st
Associate II
Posted on March 02, 2015 at 15:36

Erwan

I have tried the image programmed into the board from factory (flashing LED example). This boots from Flash as expected. One of the differences between this and my image is that the factory build does not start with VLE instructions. Is this a limitation?

Thanks

Kevin

kevin239955_st
Associate II
Posted on March 02, 2015 at 18:07

Erwan

Slight update on the above: our code isn't disabling the (SWT) watchdog on startup. I think this may be the problem...

Kevin

Erwan YVIN
ST Employee
Posted on March 02, 2015 at 18:46

Hello Kevin ,

Warning, the device BXX supports only the VLE mode.

Anyway , for the WD, it is on the Debugger configuration after the Reset

// disable watchdog

SET SWT_SR 0xC520

SET SWT_SR 0xD928

SET SWT_CR 0xFF00000A

Best Regards

                      Erwan