cancel
Showing results for 
Search instead for 
Did you mean: 

Best way to stop ATOM output on critical fault?

jmary
Associate III

Using SPC572 GTM for ecu, what is the best way to stop ATOM output in critical fault?

Already tried to stop the GTM, but on re initialize the result is unpredictable. 

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

i recommend to check the application in SPC5Studio Tool Suite it is a good example

SPC572Lxx_RLA GTM DPLL Test Application for Discovery

ErwanYVIN_0-1692781103340.png

Do you have access to http://gtm.spc5studio.com (Update Site) ?

If not , send your request in credentials@spc5studio.com

               Best Regards

                                Erwan

View solution in original post

7 REPLIES 7
Erwan YVIN
ST Employee

Hello ,

i recommend to check the application in SPC5Studio Tool Suite it is a good example

SPC572Lxx_RLA GTM DPLL Test Application for Discovery

ErwanYVIN_0-1692781103340.png

Do you have access to http://gtm.spc5studio.com (Update Site) ?

If not , send your request in credentials@spc5studio.com

               Best Regards

                                Erwan

Yes, I already run sample from http://gtm.spc5studio.com.

the problem start when the GTM loss lock event, the code then restart and reinitialize the GTM. but then, then DPLL PMT become invalid, so the function that request PMT calculation stopped working.

so I need the proper way to restart the GTM. any suggestion to reset all the GTM register without fully restart the MCU?

Hi Erwan,

I cannot also access to http://gtm.spc5studio.com, so in order to run sample, SPC572Lxx_RLA GTM DPLL Test Application for Discovery, do I only need to send an email to credentials@spc5studio.com for authorization of this sample? Thanks!

To run SPC572Lxx_RLA GTM DPLL Test Application, the library url is http://download.spc5studio.com/updates

Install directly from default spc5 studio installation.

Hi Jmary,

Please refer to the pic below.

savant_0-1695697243749.png

then how to import SPC572Lxx_RLA GTM DPLL Test Application project? I cannot find it. Thanks!

Screenshot_1.png

Hi Jmary,

Thank you very much.