cancel
Showing results for 
Search instead for 
Did you mean: 

What other hardware can be used as a target for AlgoBuilder GUI?

Evelina CAMILLERI
ST Employee

[webinar - Program decision trees in sensors with a Machine Learning Core]

1 ACCEPTED SOLUTION

Accepted Solutions
Evelina CAMILLERI
ST Employee

Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.

A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.

View solution in original post

1 REPLY 1
Evelina CAMILLERI
ST Employee

Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.

A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.