cancel
Showing results for 
Search instead for 
Did you mean: 

what is the exact principle of time of flight technology?

esakkiraja
Associate II
Posted on December 17, 2016 at 06:48

Hi, i searched for the exact principle of the time of flight technology in internet but the answer i got was different in different websites. I bought VL53l0X sensor recently and i need the exact principle of TOF of ST's product.

2 REPLIES 2
Seb
ST Employee
Posted on December 17, 2016 at 07:10

Most of the information is in the

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/b2/1e/33/77/c6/92/47/6b/DM00279086/files/DM00279086.pdf/jcr:content/translations/en.DM00279086.pdf

:

Burst of infrared pulses from vertical laser is emitted in a cone shaped solid angle.

If there is an object, the reflected light beam will be sensed by the avalanche photo diod.

The distance is calculated by mesuring the time it took from emission to reception of a light pulse.

0.299792 mm per picosecond ==> 1mm correspond to ~3 ps time granularity implementation

Posted on December 17, 2016 at 07:25

And also one more doubt on Calibration. Is offset calibration done in any specific ranging mode such as long range, high accuracy and high speed?