2015-02-10 6:24 AM
The title really says it all.
The pin description for the LSM9DS1 says that the DEN_A/G pin is the Accelerometer/Gyroscope Data Enable. This sounds important, but I can't see anywhere in the datasheet that explains what you're meant to do with it. Can I just tie it to 3.3V, since I want data to always be enabled? Or tie it to ground? Or maybe to the CS_A/G pin, so that it only takes readings when I'm not actually communicating with it? The only thing I can't do is connect it to a microcontroller pin, because I've run out of those. Thanks for any help #data-enable #lsm9ds1 #den_a/gSolved! Go to Solution.
2019-03-10 8:24 AM
Hi All:
Does the Interrupt pins need to be pulled high?
BR