What do the self-tests of the ASM330LHH actually prove?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 12:10 PM
Hello, I hope you are well.
I had a query about the IMU ASM330LHH. I want to know whether the self-test functions of the internal accelerometer and gyroscope (see attached pictures) test the internal MEMS sensors or not. I have doubts whether these self-tests only internally generate standard values for acceleration and angular velocity without actually testing the MEMS.
Thank you very much.
Solved! Go to Solution.
- Labels:
-
INEMO-Inertial Modules
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 2:37 PM
Hello @FedIng
The embedded self-test functions allow checking the device functionality without moving it.
Also, When the accelerometer self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. In this case, the sensor outputs exhibit a change in their DC levels which are related to the selected full scale through the sensitivity value.
The accelerometer self-test function is off when the ST[1:0]_XL bits of the CTRL5_C register are programmed to 00. It is enabled when the ST[1:0]_XL bits are set to 01 (positive sign self-test) or 10 (negative sign self-test). When the accelerometer self-test is activated, the sensor output level is given by the algebraic sum of the signals produced by the acceleration acting on the sensor and by the electrostatic test-force.
For more informations about the self-test, take a look at the chapter 9 of the AN5296.
Best regards.
II
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 2:37 PM
Hello @FedIng
The embedded self-test functions allow checking the device functionality without moving it.
Also, When the accelerometer self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. In this case, the sensor outputs exhibit a change in their DC levels which are related to the selected full scale through the sensitivity value.
The accelerometer self-test function is off when the ST[1:0]_XL bits of the CTRL5_C register are programmed to 00. It is enabled when the ST[1:0]_XL bits are set to 01 (positive sign self-test) or 10 (negative sign self-test). When the accelerometer self-test is activated, the sensor output level is given by the algebraic sum of the signals produced by the acceleration acting on the sensor and by the electrostatic test-force.
For more informations about the self-test, take a look at the chapter 9 of the AN5296.
Best regards.
II
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-26 9:02 AM
¡Thank you so much @Issamos for the complete answer and the AN link!