cancel
Showing results for 
Search instead for 
Did you mean: 

VL6180X operation

sbertuletti
Associate II
Posted on March 01, 2016 at 17:10

I undesratnd that ''ST Time of Flight technology uses photon detectors to measure the time it takes a generated light pulse to leave our product, then reflect from a target and come back to our device.  Knowing the time it takes, an accurate distance measurement can be calculated knowing the speed of light.''

My question is: since VL6180X calculate the distance as the time between transmitting and receiveing the infrared, how can it measure distances (e.g. about 1cm) which correspond to a time of flight in the order of picoseconds ?

Thanks

#vl6180x
2 REPLIES 2
Julien NGUYEN
ST Employee
Posted on March 19, 2016 at 01:14

Sorry, we can not tell you. It is a ST IP.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
John E KVAM
ST Employee
Posted on January 02, 2018 at 20:08

The answer is statistics. There are almost a million small pulses of light and a rather complex statistical algorithm to figure it all out. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.