2021-03-08 6:35 AM
Dear Team,
We are using VL53l1X in our application to detect people leaving and entry, we got 5 vl53l1x breakout boards from one of my distributors for prototyping.
People count programming working without any issues when using it in polling/continuous mode, but for power optimization we want to use an interrupt method, Count increment and decrement should happen when there is an interrupt, rest of the time the main controller and other things to be in sleep mode.
Here is the code...
//Event CallBack
void interrupt_handler(nrf_drv_gpiote_pin_t pin, nrf_gpiote_polarity_t action)
{
nrf_drv_gpiote_in_event_disable(INTERRUPT_PIN);
event = true;
printf("Event occured\n");
}
//Main code
int main(void)
{
uint8_t byteData, sensorState=0;
uint16_t wordData;
uint16_t Distance, Signal;
uint8_t RangeStatus;
uint8_t dataReady;
uint8_t intPolarity;
int PplCounter;
int center[2] = {FRONT_ZONE_CENTER, BACK_ZONE_CENTER}; /* these are the spad center of the 2 4*16 zones */
//int Zone = 0;
gpio_init();
printf("\r\nTWI sensor example started.\n");
twi_init();
detect_slave_device();
// Those basic I2C read functions can be used to check your own I2C functions */
status = VL53L1_RdByte(dev, 0x010F, &byteData);
printf("VL53L1X Model_ID: %X\n", byteData);
status = VL53L1_RdByte(dev, 0x0110, &byteData);
printf("VL53L1X Module_Type: %X\n", byteData);
status = VL53L1_RdWord(dev, 0x010F, &wordData);
printf("VL53L1X: %X\n", wordData);
while (sensorState == 0) {
status = VL53L1X_BootState(dev, &sensorState);
nrf_delay_ms(2);
}
printf("Chip booted\n");
status = VL53L1X_SensorInit(dev);
status += VL53L1X_SetDistanceMode(dev, DISTANCE_MODE); /* 1=short, 2=long */
status += VL53L1X_SetTimingBudgetInMs(dev, TIMING_BUDGET); /* in ms possible values [15, 20, 50, 100, 200, 500] */
status += VL53L1X_SetInterMeasurementInMs(dev, TIMING_BUDGET);
status += VL53L1X_SetROI(dev, ROWS_OF_SPADS, 16); /* minimum ROI 4,4 */
if (status != 0) {
printf("Initialization or configuration of the device\n");
return (-1);
}
VL53L1X_SetInterruptPolarity(dev, 0);
VL53L1X_SetDistanceThreshold(dev,50,1000,3,0);
VL53L1X_GetInterruptPolarity(dev, &intPolarity);
printf("Interrupt mode : %d\n", intPolarity);
printf("Start counting people with profile : %s...\n", PROFILE_STRING);
status = VL53L1X_StartRanging(dev);
while(1)
{
if(event == true){
status += VL53L1X_GetRangeStatus(dev, &RangeStatus);
status += VL53L1X_GetDistance(dev, &Distance);
status += VL53L1X_GetSignalPerSpad(dev, &Signal);
//event = false;
status += VL53L1X_ClearInterrupt(dev);
if (status != 0) {
printf("Error in operating the device\n");
return (-1);
}
status = VL53L1X_SetROICenter(dev, center[Zone]);
if (status != 0) {
printf("Error in chaning the center of the ROI\n");
return (-1);
}
if ((RangeStatus == 0) || (RangeStatus == 4) || (RangeStatus == 7)) {
if (Distance <= MIN_DISTANCE) // wraparound case see the explanation at the constants definition place
Distance = MAX_DISTANCE + MIN_DISTANCE;
}
else // severe error cases
Distance = MAX_DISTANCE;
PplCounter = ProcessPeopleCountingData(Distance, Zone, RangeStatus);
Zone++;
Zone = Zone%2;
}
}
}
Making event = false and nrf_drv_gpiote_in_event_enable(INTERRUPT_PIN) , when there is a entry or exit or wrong path.
Please provide with us VL53L1X APIs for interrupt method.
Thanks & Regards
Mariswamy M
AXISCADES Engineering Technologies PVT Ltd, Bangalore
mariswamy.m@axiscades.com
Solved! Go to Solution.
2021-09-07 11:58 AM
This is a hard one.
Interrupt mode will save some MCU power, but it won't save any power in the sensor.
The sensor uses about 20mA while it's running. Most of that power is used to power the Laser.
A range generally takes about 20ms and if you range 10 times per second you are going to use 20mA * 0.020 seconds *10 runs.
It's going to use this power, interrupt or polling.
You can only save power by reducing the Timing Budget, or the number of time you range per second.
In autonomous mode, the sensor will quite happily run and generate an interrupt only when a threshold you set is crossed.
So your MCU can be asleep, waking only on the receipt of an interrupt.
But if you range fewer times to save power, I'm going to guess you will miss people walking by.
2021-09-07 11:58 AM
This is a hard one.
Interrupt mode will save some MCU power, but it won't save any power in the sensor.
The sensor uses about 20mA while it's running. Most of that power is used to power the Laser.
A range generally takes about 20ms and if you range 10 times per second you are going to use 20mA * 0.020 seconds *10 runs.
It's going to use this power, interrupt or polling.
You can only save power by reducing the Timing Budget, or the number of time you range per second.
In autonomous mode, the sensor will quite happily run and generate an interrupt only when a threshold you set is crossed.
So your MCU can be asleep, waking only on the receipt of an interrupt.
But if you range fewer times to save power, I'm going to guess you will miss people walking by.