2017-08-11 01:20 AM
Dear,all:
ST companies have used for vibration measuring acceleration sensor? Requirements are as follows:
Frequency response: more than 1khRange: 0-40 gPower:Low power consumptionUsed in water pump, fan and other industrial sitesif ST companies have not these sensor,Can you introduce other company sensor?
2017-08-14 02:22 AM
You can consider
http://www.st.com/content/st_com/en/products/mems-and-sensors/accelerometers/h3lis331dl.html
the range is 100/200/400g, but the maximum output data rate is only 1kHz.Are you sure you need to measure vibration up to 40g? If 16g would be enough you can also consider
http://www.st.com/content/st_com/en/products/mems-and-sensors/accelerometers/iis2dh.html
which is capable to provide data with output data rate up to 5376 Hz.2017-12-11 08:35 PM
Thanks your response!
The IIS2DH' ADC is 12bit,i think the
2017-12-12 03:40 AM
You can check this overview of ST accelerometers.