2024-01-27 09:44 AM
Hello,
I have STEVAL-MKI236A (ASM330LHB - IMU) evaluation board, How can I make use of the UNICO-GUI to interface with the board. I do see the board listed on the GUI but how will I be able to interface with gui with just I2C without using the MOTHERBOARDs.
Thanks!
2024-01-29 02:44 AM
Hi @govindrzook ,
Are you using the STEVAL MKI109V3?
2024-01-30 09:38 AM
Hello @Federica Bossi
I am not making use of STEVAL-MKI109V3 motherboard and currently directly using the evaluation board via SCL, SDA pins of I2C interface. is it possible to make use of the UNICO-gui without that motherboard?
Please advise thanks!
2024-02-01 02:23 AM
Hi @govindrzook ,
Yes, as explained in our official page, it is available for three operating systems: STSW-MKI109L for Linux Debian-based; STSW-MKI109M for Mac OS X; STSW-MKI109W for Windows.