2024-08-31 10:19 PM
I am trying to use IKS4A1 with IDB05A2 together with F446RE.
Each of these expansion boards works fine with F446RE. However, when I try to use STM32CubeMX to create a combined project, I cannot add the BLE1_applications.
I assume this configuration should work so I can use MEMS data over a BLE1. Is my assumption correct?
If yes, then what is the best way to solve my issue in STM32CubeMX?