2017-02-03 6:36 PM
Hi,
We are developing a ultra low power sensor module with the LSM303D. The LSM303D was periodically waken up to take a magnetic and temperature measure (no acceleration measurment). The total excepted average current is <100uA, but the acture current is >300uA which was unacceptable.
The following picture was snapped from the oscilloscope measuring the module's current. The narrow pulse current were caused by the module's periodically magnetic and temperature measuring activity. But the ramp shape pulses were unexpected. Sicne these ramp-pulse lasts for hundreds of miniseconds each, the total current was dramatically increased.
The questions is:
Are these ramp-pules current normal for the LSM303D?
The following source code is for the periodically measuring:
int8 fLSM_TakeOneMeasure(int16 *pAccXYZ, int16 *pMagXYZ, int16 *pTemp)
{ int8 rt; uint8 RegVal;//Unsupported, no acc measurment
if(pAccXYZ!=NULL){ return -1; }if((pMagXYZ!=NULL)||(pTemp!=NULL)){
//Config //CTRL1 RegVal=0x08; //AODR: 0000 (Acceleration data-rate selection: 0000: Power-down mode) //BDU: 1 (Block data update for acceleration and magnetic data: 0: continuous update; 1: output registers not updated until MSB and LSB have been read) //AZEN: 0 (Acceleration Z-axis enable: 0: disabled; 1: enabled) //AYEN: 0 (Acceleration Y-axis enable: 0: disabled; 1: enabled) //AXEN: 0 (Acceleration X-axis enable: 0: disabled; 1: enabled) rt=fLSM_WriteReg(LSM_CTRL1,RegVal); if(rt!=0){return 2;} //CTRL5 RegVal=0xE0; //TEMP_EN: 1 (Temperature sensor enabled.) //M_RES: 11 (Magnetic resolution: 00: low resolution, 11: high resolution) //M_ODR: 000 (Magnetic data rate: 000-3.125 Hz�?110-Do not use) //LIR2: 0 (Latch interrupt request on INT2_SRC register: not latched) //LIR1: 0 (Latch interrupt request on INT1_SRC register: not latched) rt=fLSM_WriteReg(LSM_CTRL5,RegVal); if(rt!=0){return 2;}//CTRL7
RegVal=0x00; //AHPM: 00 (High-pass filter mode selection for acceleration data: Normal mode) //AFDS: 0 (Filtered acceleration data selection: internal filter bypassed) //T_ONLY: 0 (Temperature sensor only mode: OFF ) //Rsv: 0 //MLP: 0 (Magnetic data low-power mode: 0-OFF�?1-ON) //MD: 01 (Magnetic sensor mode: 00-Continuous�?01-Single�?10-Powerdown�?11-Powerdown) rt=fLSM_WriteReg(LSM_CTRL7,RegVal); if(rt!=0){return 2;} //Read if(pMagXYZ!=NULL){ //Readout while(1){ RegVal=fLSM_ReadReg(LSM_STATUS_M); if((RegVal&0x0F)==((uint8)0x0F)){ break; } SLEEP(1); } //x RegVal=fLSM_ReadReg(LSM_OUT_X_H_M); pMagXYZ[0]=RegVal;pMagXYZ[0]<<=8; RegVal=fLSM_ReadReg(LSM_OUT_X_L_M); pMagXYZ[0]|=RegVal; //y RegVal=fLSM_ReadReg(LSM_OUT_Y_H_M); pMagXYZ[1]=RegVal;pMagXYZ[1]<<=8; RegVal=fLSM_ReadReg(LSM_OUT_Y_L_M); pMagXYZ[1]|=RegVal; //z RegVal=fLSM_ReadReg(LSM_OUT_Z_H_M); pMagXYZ[2]=RegVal;pMagXYZ[2]<<=8; RegVal=fLSM_ReadReg(LSM_OUT_Z_L_M); pMagXYZ[2]|=RegVal; } if(pTemp!=NULL){ RegVal=fLSM_ReadReg(LSM_TEMP_OUT_H); *pTemp=RegVal;*pTemp=(*pTemp)<<8; RegVal=fLSM_ReadReg(LSM_TEMP_OUT_L); *pTemp=(*pTemp)|RegVal; } //Shutdown //CTRL7 RegVal=0x02; //AHPM: 00 (High-pass filter mode selection for acceleration data: Normal mode) //AFDS: 0 (Filtered acceleration data selection: internal filter bypassed) //T_ONLY: 0 (Temperature sensor only mode: OFF ) //Rsv: 0 //MLP: 0 (Magnetic data low-power mode: OFF) //MD: 10 (Magnetic sensor mode: 00-Continuous�?01-Single�?10-Powerdown�?11-Powerdown) rt=fLSM_WriteReg(LSM_CTRL7,RegVal); if(rt!=0){return 2;} //CTRL5 RegVal=0x60; //TEMP_EN: 0 (Temperature sensor enabled.) //M_RES: 11 (Magnetic resolution: 00: low resolution, 11: high resolution) //M_ODR: 000 (Magnetic data rate: 000-3.125 Hz�?110-Do not use) //LIR2: 0 (Latch interrupt request on INT2_SRC register: not latched) //LIR1: 0 (Latch interrupt request on INT1_SRC register: not latched) rt=fLSM_WriteReg(LSM_CTRL5,RegVal); if(rt!=0){return 2;} } return 0;}2017-02-06 2:20 AM
According to the datasheet the 300uA is typical current consumption.
See Table 5. below.
How did you get your estimation 100uA ?
I suppose the ramp-pulses are caused by demagnetization of the magnetic sensor for each measurement to improve the accuracy.