2018-05-14 07:11 AM
Posted on May 14, 2018 at 16:11
Hello, can you please tell if the temperature sensor on ISM330DLC returns absolute temperature values or the difference values with respect to a reference? Just read a thread (
https://community.st.com/0D50X00009XkXfjSAF
) that mentions 'difference with respect to a reference' so wanted to confirm if the same is happening for ISM330DLC as well.
Best regards,
Ankur
2018-05-14 07:53 AM
Here are the temperature sensor characteristics from the device datasheet.
As you can see the sensors measure difference values with respect to reference 25°C. The offset can be up to +/- 15°C.
2018-05-14 10:41 PM
Thanks Miroslav. So if we have multiple devices with this sensor, every device can have a different temperature offset, correct?
2018-05-15 03:08 PM
Yes, it is correct.
2018-05-16 06:58 AM
Thanks Miroslav!