cancel
Showing results for 
Search instead for 
Did you mean: 

Temperature sensor on ISM330DLC

Ankur Shanker
Associate II

Posted on May 14, 2018 at 16:11

Hello, can you please tell if the temperature sensor on ISM330DLC returns absolute temperature values or the difference values with respect to a reference? Just read a thread (

https://community.st.com/0D50X00009XkXfjSAF

) that mentions 'difference with respect to a reference' so wanted to confirm if the same is happening for ISM330DLC as well.

Best regards,

Ankur

4 REPLIES 4
Miroslav BATEK
ST Employee
Posted on May 14, 2018 at 16:53

Here are the temperature sensor characteristics from the device datasheet.

As you can see the sensors measure difference values with respect to reference 25°C. The offset can be up to +/- 15°C.

0690X0000060KkGQAU.png
Ankur Shanker
Associate II
Posted on May 15, 2018 at 07:41

Thanks Miroslav. So if we have multiple devices with this sensor, every device can have a different temperature offset, correct?

Posted on May 15, 2018 at 22:08

Yes, it is correct.

Posted on May 16, 2018 at 13:58

Thanks Miroslav!