2021-09-08 4:18 AM
On the STEVAL-STWINKT1B board, and using the HSDatalog firmware, it uses about 60mA in idle state. I have disconnected the sensors, and the uC, and turned off the SD card power lines, but it's still at around 2mA. Does anyone know where this power is going? Ideally, I want to create an application for the board when it wakes up for 1 minute in every hour, logs the data to the SD card, and then goes into a nearly dormant low power state to preserve the battery.
Solved! Go to Solution.
2021-09-09 8:30 AM
Hi @LWeir.775 ,
In the current design, unfortunately, the 2.7A regulator cannot be switched OFF, so also the connected OpAmp is always ON.
The only option would be to de-solder it, or de-solder the OpAmp which accounts for more than 1mA alone.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-09-09 8:30 AM
Hi @LWeir.775 ,
In the current design, unfortunately, the 2.7A regulator cannot be switched OFF, so also the connected OpAmp is always ON.
The only option would be to de-solder it, or de-solder the OpAmp which accounts for more than 1mA alone.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-09-09 8:46 AM
2021-09-10 1:56 AM
Hi @LWeir.775 ,
The DCDC converter provides the supply the microphone, so this would be the only component that would be excluded removing the LDO.
We are however designing a rev2 platform, and we will take it into account this issue.
-Eleon
2021-09-10 2:04 AM
2021-09-10 7:28 AM
Hi Laurence,
I cannot disclose a precise timeline for this application, but it will be in the next months.
-Eleon
2021-09-10 7:38 AM