cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-MKBOXPRO firmware that is compatible with ISPU dil24

benx1326
Associate II

I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a screenshot of the current firmware I'm using FPSNS DATALOG 2 in which it shows the ispu as unknown and if I try to upload the UCF it's just gets stuck!

 

1 REPLY 1
Federica Bossi
ST Employee

Hi @benx1326 ,

Welcome to ST Community!

Unfortunately ISM330IS firmware for STEVAL-MKBOXPRO is not currently available. We are working on it and it will release in future.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.