cancel
Showing results for 
Search instead for 
Did you mean: 

State Machine and stack size ?

antonius
Senior

Dear Members,

I have a state machine but it seems that it stuck in one state,

Is it related with stack size ?

It's stuck on "case PULSE_IDLE" no matter the value of sensor_value,

The code :

switch(currentPulseDetectorState)
  {
    case PULSE_IDLE:
      if(sensor_value >= PULSE_MIN_THRESHOLD) {
				//printf("Sensor_value PULSE_IDLE %f \r\n",sensor_value);
        currentPulseDetectorState = PULSE_TRACE_UP;
				
        values_went_down = 0;
				printf("PULSE IDLE\r\n");
				return true;
      }
      break;
 
    case PULSE_TRACE_UP:
			printf("Sensor value PULSE_TRACE_UP %f\r\n",sensor_value);
      if(sensor_value > prev_sensor_value)
      {
				
        printf("PULSE TRACE_UP\r\n");
				currentBeat =HAL_GetTick();
        lastBeatThreshold = sensor_value;
				
				
      }
      else
      {
 
         printf("Peak reached: ");
          printf("%f \r\n",sensor_value);
          printf(" ");
          printf("%f \r\n",prev_sensor_value);      
 
        uint32_t beatDuration = currentBeat - lastBeat;
        lastBeat = currentBeat;
 
        float rawBPM=0;
        if(beatDuration > 0)
          rawBPM = 60000.0 / (float)beatDuration;
        printf("RawBPM = %f\r\n",rawBPM);
 
        //This method sometimes glitches, it's better to go through whole moving average everytime
        //IT's a neat idea to optimize the amount of work for moving avg. but while placing, removing finger it can screw up
        //valuesBPMSum -= valuesBPM[bpmIndex];
        //valuesBPM[bpmIndex] = rawBPM;
        //valuesBPMSum += valuesBPM[bpmIndex];
 
        valuesBPM[bpmIndex] = rawBPM;
        valuesBPMSum = 0;
        for(int i=0; i<PULSE_BPM_SAMPLE_SIZE; i++)
        {
          valuesBPMSum += valuesBPM[i];
        }
 
       
 
        bpmIndex++;
        bpmIndex = bpmIndex % PULSE_BPM_SAMPLE_SIZE;
 
        if(valuesBPMCount < PULSE_BPM_SAMPLE_SIZE)
          valuesBPMCount++;
 
        currentBPM = valuesBPMSum / valuesBPMCount;
        
          printf("AVg. BPM: ");
          printf("%f",currentBPM);
        
 
 
        currentPulseDetectorState = PULSE_TRACE_DOWN;
 
        return true;
      }
      break;
 
    case PULSE_TRACE_DOWN:
      if(sensor_value < prev_sensor_value)
      {
        values_went_down++;
      }
 
 
      if(sensor_value < PULSE_MIN_THRESHOLD)
      {
        currentPulseDetectorState = PULSE_IDLE;
      }
      break;
  }
 
  prev_sensor_value = sensor_value;

Any clues on solving it ? thanks

2 REPLIES 2
Ozone
Lead III

Almost certrainly not.

With a stack problem, you would end up in the hardfault handler.

Perhaps your "sensor_value" is always less then PULSE_MIN_THRESHOLD ?

Data 7 Output MAX30100,0x09 register (FIFO DATA) IR : 1536 
                   
DC filterIR = -1147.117188
                                                    
MeanDiff filterIR = 52967.000000
                                              
LowPass filterIR = 12989.482422
                                               
Timestamp After IRRED data= 25885 
                                            
sensor_value > PULSE_MAX_THRESHOLD
                                            
Sensor_value PULSE_MAX_TRESHOLD 12989.482422 
                                 
Sensor_value at PULSE_IDLE 12989.482422 
                                      
PULSE IDLE
   
 

code :

switch(currentPulseDetectorState)
  {
    case PULSE_IDLE:
      if(sensor_value >= PULSE_MIN_THRESHOLD) {
				printf("Sensor_value at PULSE_IDLE %f \r\n",sensor_value);
       
				
        values_went_down = 0;
				printf("PULSE IDLE\r\n");
				 currentPulseDetectorState = PULSE_TRACE_UP;
				//return currentPulseDetectorState = PULSE_TRACE_UP;
      }
      break;

#define PULSE_MIN_THRESHOLD        300

I don't understand why ?