2023-07-03 2:12 PM
I have purchased the SensorTile.box Pro from Mouser, and the device is excellent to work with on coding. I have loaded 0x0000000 with bin file default from F:\ST_SensorTile_Box_Pro\STM32CubeFunctionPack_STBOX1_V1.5.0\Projects\STWIN.box\Applications\DefaultFw\Binary\DefaultFw.bin
The SensorTile.box Pro does not work and is unable to access the Android to start the Dice or Compass demo.
How can I get the SensorTile.box Pro back on the day I purchased it on July 27, 2023.
Best Regards,
Rob
Solved! Go to Solution.
2023-11-20 5:46 PM
I may have to just deposit 0x00 at address 0x08000000.