2018-10-21 1:20 PM
Hi,
Does the iNEMO sensor fusion tool work with accelerometers with larger than +-16g output
2018-10-22 5:06 AM
What you mean by "iNEMO sensor fusion tool"?
2018-10-22 5:40 AM
Hi,
Sure, I'm pretty much new to the ST tool chain. I'd interpreted that the software GUI, iNemo (I'm not sure if that's the software tools name), enabled a developer to select ST components in order to build a custom IMU using code auto generated from the tool.
Have I interpreted that correctly?
Thanks,
Joe.
2018-10-24 2:42 AM
Do you have a link to the tool or screenshot? I'm still not sure if you are referring to an existing tool or you are asking for such a tool?
2018-10-24 2:56 AM
Its called algobuilder
2018-10-24 2:57 AM
2018-10-24 5:26 AM
AlgoBuilder supports only X-NUCLEO-IKS01A2 or SensorTile which utilize sensors with maximum range 16g. Theoretically you could modify the FW to work with other sensor with higher range, but the functionality is not guaranteed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.