2022-05-08 8:05 PM
As per the Release Notes (v2.4.0 / 5-Nov-2021) for HS DataLog CLI example, I could see executable and libs are present under directory Utilities/cli_example for Raspberry Pi 3B. I have also exported and set the shared library path using command.
export LD_LIBRARY_PATH=<Utilities/cli_example/bin>
But when I execute below command
./bin/cli_example_rpi3b -f ../STWIN_config_examples/DeviceConfig.json -t 100
I am getting following error error.
./cli_example_rpi3b: error while loading shared libraries: libhs_datalog.so: wrong ELF class: ELFCLASS64
Could you please advise whether I am doing anything wrong?
2022-07-22 2:08 AM
Hi @digidhamu,
To overcome any kind of configuration issues, we will provide a configuration script for linux and raspberry in the FP-SNS-DATALOG1 v1.4.0.
This new version will be available by the end of July/first days of August.
You will just lunch the raspberry_setup/setup_rpi3b.sh script, and then everything should work properly.
I suggest you to update the CLI once available.
In your use case, you are loading the entire /bin folder, that contains both Linux and Raspberry .so version.
The Linux one (libhs_datalog.so) can't work on Raspberry and maybe that's the reason for the error.
Move libhs_datalog.so into another folder and launch newly the script.
Do you still have the same error?
Best regards