cancel
Showing results for 
Search instead for 
Did you mean: 

Resistor changes for STEVAL-MKI196V1 and STEVAL-MKI109V2

MSack.1
Associate

Hi,

On the MKI196V1 webpage (https://www.st.com/en/evaluation-tools/steval-mki196v1.html) It says that:

"Changing the resistor settings is also compatible with the STEVAL-MKI109V2 motherboard"

I cannot find any documentation on which resistor changes are required. Currently I am getting the following error from Unico:

0693W000006EONBQA4.png 

Does anyone know how to fix this?

Thanks

Matt

1 REPLY 1
Peter BENSCH
ST Employee

You are currently connecting the STEVAL-MKI196V1 to the STEVAL-MKI109V2, right?

The STEVAL-MKI196V1 is compatible with the STEVAL-MKI109V3 due to the 4 resistors (zero ohm bridges) R1, R3, R5 and R7 set per default.

You need to unsolder these resistors and instead set the 0 ohm jumpers at R2, R4, R6 and R8 so that the STEVAL-MKI196V1 can be used with your STEVAL-MKI109V2.

The schematics of these tools can be found in the documentation tab of the websites linked above.

Good luck!

When your question is answered, please close this topic by choosing Select as Best.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.