Questions about how IKS01A3 DataLogTerminal example works
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-04 6:49 AM
Hi,
I'm using the IKS01A3 board on a P-NUCLEO-WB55 board with the example application IKS01A3 DataLogTerminal.
Some questions:
- where is the mapping from GPIO numbers (0 through 15) to pin names on the micro (STM32WB55 in QFN68 package)? I have the board schematic which shows port names e.g. PA0, etc. but the example code refers to GPIO numbers. I can't find the mapping from GPIO numbers to pin/port names.
- I'm trying to see all of the LIS2DW12 sensor data, not just a 1s sample as done in the MX_IKS01A3_DataLogTerminal_Process function in the app_mems.ca file. I can't see where the interrupt service routine reads the sensor and writes it into the IKS01A3_MOTION_SENSOR_Axes_t data structure.
Thanks for helping a newbie!
Jim Tompkins
Halifax, Canada
Solved! Go to Solution.
- Labels:
-
STM32WB series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-21 1:58 AM
Hi Jim @JTomp.1 ,
sorry, it is the FP-SNS-MOTENVWB1 function pack (not the FP-SENS-MOTENV1), which is dedicated to the P-NUCLEO-WB55 + X-NUCLEO-IKS01A3.
-Eleon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-10 4:24 AM
Hi Jim @JTomp.1 ,
- to match the GPIO name with the STM32WB55 pin, you can use the STM32CubeMX tool for the uC configuration, where the STM32WB55 default configuration is implemented.
- Are you using Unicleo-GUI for the data acquisition? Did you try to use the \Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1 example in the FP-SNS-MOTENV1 firmware function pack, which combines the P-NUCLEO-WB55 board with the IKS01A3 expansion?
Let me know if these suggestion can help your application building.
-Eleon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-10 8:49 AM
Hi Eleon,
Thanks for the answer!
I will look in MX for the pin configurations. In the image above, for example, PB0 has signal name = GPIO-Output. The code refers to GPIO0: GPIO15. I was hoping to find a reference somewhere in the code from PB0 to one of the GPIOx names, but could not find this.
I downloaded the FP-SENS-MOTENV1 function pack to try. Under projects, I can't see a reference to STM32WB55. Also, if I start a new project in MX using the P-NUCLEO-WB55 board and try to add embedded software packs using the FP-SENS-MOTENV1 .zip file, it doesn't like the format of the .zip file. Does FP-SENS-MOTENV1 support P-NUCLEO-WB55?
The DataLogTerminal example works, but I would like to modify in as follows for my own application:
- use only the LIS2DW12 sensor on the IKS01A3. I couldn't see easily which interrupt was used for which sensor. When I disabled all the interrupts listed in MX_GPIO_INIT in main.c, the application still worked! So I'm not clear how the data gets from the sensor into the micro. Is it polled?
- log all of the LIS2DW12 X, Y and Z data into a circular buffer and then do some processing on it. But I can't see in the code where the LIS2DW ISR grabs the data from the sensor.
Thanks for your help,
Jim
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-11 5:02 AM
Hi @JTomp.1 ,
my suggestion to start from the project in: \Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1\STM32CubeIDE\MOTENV1_IKS01A3_WB55RG, opening it with the STM32CubeIDE or the the IDE you use, instead of from the CubeMX trying to import the firmware package in .zip file format.
On this project, the LIS2DW12 is implemented and you can disable all the other sensors if you need.
As regard the DataLogTerminal example, yes, the data acquisition from the sensor is in polling mode: if you want to trigger it you should insert the function below in a loop as defined in lis2dw12_read_data_single.c:
int32_t LIS2DW12_ACC_GetAxes(LIS2DW12_Object_t *pObj, LIS2DW12_Axes_t *Acceleration)
-Eleon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-11 6:57 AM
Hi Eleon,
My STM32Cube_FW_WB_V1.9.0 installation doesn't include the MOTENV1 application folder. See the image above.
My installation of the MOTENV1 function pack doesn't have a subfolder for the P-NUCLEO-WB55.
Do I need to install something else?
I will take a look at the read_data_single C file.
Thanks,
Jim
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-21 1:58 AM
Hi Jim @JTomp.1 ,
sorry, it is the FP-SNS-MOTENVWB1 function pack (not the FP-SENS-MOTENV1), which is dedicated to the P-NUCLEO-WB55 + X-NUCLEO-IKS01A3.
-Eleon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-21 5:51 AM
Best regards,
Jim