2021-09-17 7:15 PM
Hello, I’m using the IIS3DWB with an Arduino Portenta, using a procedure similar to Kris Winer’s github (i.e. using the FIFO buffer in continuous mode, 256 watermark, stop on watermark, data ready interrupt on watermark, running various cycles until having all the required samples for FFT).
Reading FREQ_FINE from the INTERNAL_FREQ_FINE register doesn’t seems to work. It gives 0 when I read those bits (I tried reading from the register in different parts of the code).
Can you give me an advice on how to make it work? I made sure to have 1 in the variable that receives the value from FREQ_FINE[7:0] bits, in order to see if the 0 was really the read from INTERNAL_FREQ_FINE register.
I wanted to check the sampling frequency since in my experiments it seems to be slightly different to 26667 Hz. And I came to the problem of not being able to have information from INTERNAL_FREQ_FINE register
Many thanks in advance!
2021-09-28 2:44 AM
Hi @FCook.1 ,
let me ask you some question to better understand the situation:
how are you reading the register?
is the read of the INTERNAL_FREQ_FINE register the same as other read performed in the code?
Niccolò
2021-09-28 7:15 PM
Hi Niccolò, I'm reading as follows:
#define IIS3DWB_INTERNAL_FREQ_FINE 0x63
....
uint8_t IIS3DWB::readByte(uint8_t reg)
{
SPI.beginTransaction(SPISettings(IIS3DWB_SPI_CLOCK, MSBFIRST, IIS3DWB_SPI_MODE));
digitalWrite(_cs, LOW);
SPI.transfer((reg & 0x7F) | 0x80);
uint8_t temp = SPI.transfer(0);
digitalWrite(_cs, HIGH);
SPI.endTransaction();
return temp;
}
....
uint8_t IIS3DWB::getFreq()
{
uint8_t temp = readByte(IIS3DWB_INTERNAL_FREQ_FINE); // read freq register
return temp;
}
Other parts of the code use readBytes, so that part of the code is OK. I've tried using the getFreq function in different parts of the code and the answer is 0.
PS: I've stoped using the FIFO and now using the sensor only in bypass mode, it seems to me simpler to implement. With the FIFO I had missing values when looping after the buffer is full.
Regards,