Problem with L3G4200 Sensor using I2C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-28 2:51 AM
I have a problem interfacing with L3G4200 using I2C on STM32F469 Discovery. Here is my code to config the I2C
void I2CConfig(void){
I2CHandle1.Instance = I2Cx;
I2CHandle1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
I2CHandle1.Init.ClockSpeed = 100000;
I2CHandle1.Init.DutyCycle = I2C_DUTYCYCLE_2;
I2CHandle1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
I2CHandle1.Init.OwnAddress1 = 0xD0;
I2CHandle1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
I2CHandle1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
if (HAL_I2C_Init(&I2CHandle1) != HAL_OK)
Error_Handler();
}
And here is the code to initialize the I2C on HAL_Init file
void HAL_I2C_MspInit(I2C_HandleTypeDef *hi2c){
GPIO_InitTypeDef GPIO_InitStruct;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock */
I2Cx_SCL_GPIO_CLK_ENABLE();
I2Cx_SDA_GPIO_CLK_ENABLE();
/* Enable I2Cx clock */
I2Cx_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* I2C TX GPIO pin configuration */
GPIO_InitStruct.Pin = I2Cx_SCL_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Alternate = I2Cx_SCL_SDA_AF;
HAL_GPIO_Init(I2Cx_SCL_GPIO_PORT, &GPIO_InitStruct);
/* I2C RX GPIO pin configuration */
GPIO_InitStruct.Pin = I2Cx_SDA_PIN;
GPIO_InitStruct.Alternate = I2Cx_SCL_SDA_AF;
HAL_GPIO_Init(I2Cx_SDA_GPIO_PORT, &GPIO_InitStruct);
}
I can't figure out where is the problem because I successfully interfaced i2c using another sensor (BMP180) and also interfaced SPI with the L3G4200 with the same board.
Solved! Go to Solution.
- Labels:
-
Gyroscopes
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-29 1:10 AM
Hi,
I2C is an open drain interface, neither the master nor the slave shall pull the bits high.
External pull-up resistors are required for both I2C clock and data pins. The pins can only be pulled down when needed.
So, please instead use:
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
Best Regards,
Winfred
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-29 1:10 AM
Hi,
I2C is an open drain interface, neither the master nor the slave shall pull the bits high.
External pull-up resistors are required for both I2C clock and data pins. The pins can only be pulled down when needed.
So, please instead use:
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
Best Regards,
Winfred