cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSR use FIFO mode read data failed

sunyu
Associate

I use LSM6DSR,  I set Accelerometer ODR selection can read data, but i choose fifo mode to read data, i don't read data, i set CTRL3_C is 0x01, CTRL1_XL is 0x50,  CTRL3_C is 0x40, CTRL5_C is 0x20, CTRL9_XL is 0xf8, INT1_CTRL is 0x01, INT2_CTRL is 0x08, CTRL6_C is 0xc8,  FIFO_CTRL1 is 0xc8, FIFO_CTRL2 is 0x90, FIFO_CTRL3 is 0x05, FIFO_CTRL4 is 0xf6, Is there something wrong with my settings? 

1 REPLY 1
Federica Bossi
ST Employee

Hi @sunyu ,

You can try to follow this official example on github.

Let me know if this solves.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.