2023-04-15 11:29 AM
Hello,
I'm trying to set up the two interrupts on the LSM6DSOX, INT1 and INT2 to indicate Single and Double Tap events, respectively.
I'm able to make both events trigger their respective interrupt, but would like them to be completely separate.
I think I need to implement a delay on the Single Tap, to ensure it doesn't operate under double tap condition - it currently operates twice for a double tap!
Is there a way I can do this inside the LSM6DSO, or must I differentiate the interrupts in my microcontroller?
WriteRegister( LSM6DSOX_CTRL1_XL, B01100000 ); //Set ODR to 417Hz?
WriteRegister( LSM6DSOX_CTRL4_C, B00100000 ); //Enable Tap on X,Y,Z
WriteRegister( LSM6DSOX_TAP_CFG0, B00001110 ); //Enable Tap on X,Y,Z
WriteRegister( LSM6DSOX_TAP_CFG1, B00001000 ); //Set X Threshold
WriteRegister( LSM6DSOX_TAP_CFG2, B10001000 ); //Set Y Threshold + Enable Interrupts
WriteRegister( LSM6DSOX_TAP_THS_6D, B10001000 ); //Set Z Threshold
WriteRegister( LSM6DSOX_INT_DUR2, B01111111 ); //Set Duration/Quiet/Shock
WriteRegister( LSM6DSOX_WAKE_UP_THS, B10000000 ); //Set Wake_UP_THS for Single/Double Tap
WriteRegister( LSM6DSOX_MD1_CFG, B00000000 );
WriteRegister( LSM6DSOX_MD2_CFG, B01001000 );
Solved! Go to Solution.
2023-04-18 07:59 AM
Hi @BenG142 ,
Unfortunately it is not possible to do this inside LSM6DSOX, so I suggest you to differentiate the interrupts in your microcontroller.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster 🙂
2023-04-18 07:59 AM
Hi @BenG142 ,
Unfortunately it is not possible to do this inside LSM6DSOX, so I suggest you to differentiate the interrupts in your microcontroller.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster 🙂
2023-04-23 10:44 AM
Thank you Frederica,
Looking into writing to FIFO as a pre-conditioner!
Appreciate your reply,
Ben