cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO Register - WAKE_UP_THS - 0x5B

Dude
Associate III

Hi, 

 

I am looking at the LSM6DSO device, and I am unclear what the "USR_OFF_ON_WU" bit does in the "WAKE_UP_THS " register. Does this bit: 

  1. Drive the Wake-Up function with offset corrected accelerometer data? 0 means not offset corrected, 1 means offset corrected?
  2. What does this have to do with High-Pass Filtered Data? Does this bit actually set whether Lowpass or Highpass information is used to drive the Wakeup Function? 

 

Can someone please provide clarity? 

thanks

1 REPLY 1
Federica Bossi
ST Employee

Hi @Dude ,

When it is set to '1' the input data for the wake-up function comes from the low-pass filter path (instead of the high pass filtered data) and the programmable position is subtracted as an offset.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.